This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7811: Sample Rate vs. SPI Clock

Part Number: DAC7811


Dear Team,

our customer is looking of a DAC and the parameter search showed the DAC7811 as possible candidate.

However, we are struggling with understanding how the part with 50MHz maximum SPI clock can support a 5MSPS that is shown in the parametric search.

Since the part works with 16 bit data packages, it would reduce the 50MHz to a 50/16bit = 3.125MHz refresh - not taking the 0.2us settling time in account.

Looking forward to your feedback.

Best Regards
Martin

  • Hi Martin,

    Population of the parametric search tool is not the most intelligent system - it does not necessarily "cascade" specifications and their implications on one another or perform any sophisticated study of the implications of the timing diagrams. Essentially the sample rate shown in the table is purely drawing upon the settling time specification in the datasheet in that 1/(0.2us) = 5MHz.

    Meanwhile, your observations are true. When one takes into consideration the SPI frame requirements along with the setup and hold times with respect to SYNC rising and falling edges, plus the minimum SYNC high time the actual throughput the SPI interface limits the device to is closer to just under 3MSPS.

    In order to really push precision DAC throughput to the limit we have to consider parallel interfaces with the current portfolio, though there are some other concepts to aid with this in the roadmap which we can discuss offline.

    Can you share the customer requirements? Is supporting a parallel interface a possibility? If they're considering speeds on this magnitude I would imagine we're looking to an FPGA versus MCU / DSP so parallel may be an option.
  • Hello Kevin,
    thanks a lot for the detailed answer.
    I will reach out to you offline as soon as I have more specs.
    Best Regards
    Martin