Hello,
I'm using the ads1220 connected in a ratiometric configuration. Exc+ 5 vdc. My configuration matches the specification sheet. I also configure all four registers like the spec sheet which uses the PSW switch to power the bridge. My question regards my startup routine, which configures the registers except for config register 0 (MUX). I set this register to 1110b (AINP and AINN shorted to (AVDD + AVSS) / 2). I send the start cmd and read the output in continuous conversion mode as if I were reading the bridge normally. However, the output does not change and does not seem to be logically correct. Is there another configuration during this calibration process? Reg settings starting are 0 are: EEh, 04h, 98h, 00h for calibration.
Any help would be appreciated.
John