Part Number: ADS124S06
Dear Sir,
May I ask if Reference buffer is recommended to be enable at RTD ratiometric application?
Best regards,
Masa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS124S06
Dear Sir,
May I ask if Reference buffer is recommended to be enable at RTD ratiometric application?
Best regards,
Masa
Hi Masa-san,
this depends a little on the circuit implementation, but in general it is recommended to have the reference buffers enabled to reduce the input currents flowing into the reference inputs.
In case you place the reference resistor on the low-side (as shown in A Basic Guide to RTD Measurements, section 2.3 for example) then you could disable the reference buffer on the negative reference input if you wanted to (or have it enabled). But you should enable the reference buffer on the positive reference input.
In case the reference resistor is place on the high side (as shown in the application section of the ADS124S06 datasheet) then both reference buffers should be enabled.
Regards,