Part Number: ADS5294
Hi,
we are using 8 channel ADC = ADS5294 EVM along with ADC-to-FMC adapter to interface with KC705 board
The FMC connector voltage should be same at both the end but the KC705 FMC connector is set to 2.5 V
To interface with ADS5294 what voltage should be set in FMC connector of KC705 board ?
should it be 3.3v or 1.8 V ?
Thanks
Prateek