Part Number: ADS7223
Other Parts Discussed in Thread: ADS8363EVM
Hello Team,
we are using the ADS7223 in full clock mode. Our idea was to read the CID with each conversion for plausibility testing. It seem that in this mode the channel number reported is always "00" when CID = "0" which normally should report the Channel ID as per the description of BIT5 (CID disable) on page 35 of the datasheet. There is a hint above the diagrams on page 27 of the datasheet.
However, is there any way to read the CID when using full clock mode? Or is this feature simply not available in full clock mode?
many thanks
Lutz