need a very simple ultra low cost single channel ADC + DAC in a single package with single SPI / I2C interface.
8bit low sample rate.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eli,
We have the AMC78xx products that include both ADCs and DACs in a single package, though none of these products offer only one channel.
If you could use discrete components, the ADS7040 (8-bit, 1 MSPS SAR ADC w/ SPI) or TLA2021 (12-bit, 3.3kSPS Delta-Sigma ADC w/ I2C) are low cost ADCs that should meet your requirements.
If you can provide more detail on the need for a combined ADC+DAC, that would be helpful.