Part Number: DAC38RF80EVM
Other Parts Discussed in Thread: LMX2595, LMX2595EVM, LMK04828
Hey,
Our current system setup consists of a DAC38RF80EVM digital to analog converter, and LMX2595EVM clock synthesizer, and a Xilinx VCU108 FPGA board. My original intent was to use the LMX2595 as the master device clock for both the FPGA and the DAC (with modifications for differential clocking) dividing the clock to the correct frequency for the FPGA clock per the system parameters (line rate, lanes, etc.). However, the SMA input clock on the FPGA cannot be used for the FMC connector based on my reading. I've also looked into trying to use the user programmable clock on the FPGA as an oscillator input to the LMX2595 so that the system still shares a common clock, but there are no output terminals on the FPGA clock to tap into to send that signal to the LMX2595. It also appears that the FMC clock pins on the DAC (J2/3 or K4/5)and FPGA(G2/3 or H4/5) don't line up to transfer any clocks from one device to the other in either direction.
So my question here is, am I missing something here or did I simply choose two incompatible devices? I know that they have to share some kind of common source even if the clocks going into each are at different frequencies, but I can't seem to think of any other methods by which to do so though with my current setup.
Thoughts, comments, or recommendations would really be appreciated.
Thanks,
Jared