Dear Team,
I would like to ask how much Total Gain Error the ADS1018-Q1 has with some requested condition, FSR=+/-6.144V and Ta=-40~105C.
Thanks,
Best regards,
Koh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
I would like to ask how much Total Gain Error the ADS1018-Q1 has with some requested condition, FSR=+/-6.144V and Ta=-40~105C.
Thanks,
Best regards,
Koh
Koh-san,
The gain error for the ±6.144V range isn't specifically listed in the datasheet, but it can be inferred from other listed specifications.
Start with the maximum gain error for the ±2.048V range as ±0.25% at Ta=25°C. The maximum gain drift is 40ppm/°C. From 25°C to 105°C, there is an 80°C change and that could cause a gain error drift of 0.32%. Finally, the gain match between any two gains is 0.1%. Adding the three specifications, the maximum total gain error would be:
Max gain error = 0.25% + 0.32% + 0.1% = 0.67%
Joseph Wu
Koh-san,
The gain match is added because the min/max gain error specification is given only for the ±2.048V range. The 0.1% additional gain error comes from using the device in a different input range (in this case the ±6.144V range).
However, the gain channel match is not added because the original specification for gain error should incorporate gain error for all channels.
In the datasheet, both are listed in the electrical characterisitics table:
Joseph Wu