Part Number: ADS1120
Hello all,
I'm planning on testing the ADS1120 in an instrument system I'm working on.
The input is from one draw-wire sensor which has a single ended, unipolar DC output of 0 to 10V. The input should not fluctuate more than one mV per day.
I am planning on using a 5V VDD and using a voltage divider on the input signal to get 0-5V for maximum SNR. I plan on setting the voltage reference to VDD and disabling the PGA.
There are details about the linear range for the PGA inputs in the datasheet - does this apply for the inputs regardless of the PGA being enabled? E.g., should I expect a usable range of 0.2V to 4.8V?
Any comments appreciated, including the implementation of the anti-aliasing/input LPF.
Many thanks,
Chris