Other Parts Discussed in Thread: ADS124S08
Hi !
I want to measure a temperature with a voltage divider and a NTC thermistor. The range of the measure is 0-5V and I use a voltage reference chip (5V to supply the ADS, the voltage divider and for Vref+, Vref- set to GND).
I'll use PGA = 1, as for the range as far as I understood the datasheet if I want a full scale measure I should set Range = 0.
What I understand from the first line is that I can't have a greater difference than 2.6V between Vref+ and Vref-. Should I need a 2.5V regulator for Vref then ?
Thanks in advance,
Anthony