This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for an ADC for 48 x 48 thermopile array -IR image sensor



Hello,

I need to convert my IR image sensor (48 x 48 pixels) analog output to digital...I have just looked at LMP93601-16 bit ADC, but it supports only up to 16 x 16 pixels due to the maximum ODR of 1.3KSPS. In our case, for 48 x 48 pixels at 6 fps, we need a minimum ODR of 14 KSPS...My IR image sensor operates at 5V and the output is single ended...Please suggest if you have any solution...

Thanks,

Muthu