In my design, the DAC input pins are driven by an FPGA that has indeterminate output pins until it's powered on and not in reset. I do not have pull-up or pull-down resistors on the DAC input pins. The FPGA and the DAC are powered by separate power supplies and it's possible for the DAC to have power at Va while the FPGA is not up and stable yet. If the DAC input pins float while Va has power, do any reliability or part-damage concerns arise? Va is 4.096V and assume the input pins don't float above Va.
Thanks,
Zach