Other Parts Discussed in Thread: ADS1298ECGFE-PDK
hi team
my customer is generating a schematic for 3 lead ECG with the ADS1293
we'd like to check the following questions
1. can all the power source to the ADS1293 input at 3V ? (eg. VDD, RSTB, XTAL2, VDDIO) or must be at 3.3 and 5V? if 5V is needed is there a suggested boost IC that's commanded? (this will be 1S lithium battery application)
2. do we need RC filters before the input to IN1~IN4?? if yes, what's the suggested implementation?
3. in the figure 84, is the pin WCT and CLK not connected? is it ok to left it floating?