This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm having trouble communicating with my ADS129x device via SPI. What debug steps I should try?
If the MCU is not correctly communicating with the device, consult the Programming and SPI sections of the datasheet to review communication protocol, power-up and communication timing specifications, and pin connections. After reading the datasheet, review the steps below to find the root cause of the issue.
Review the start-up sequence and initial flow at power up (section 10.1.2 and 11.1 for the ADS1298). Some step-by-step checkpoints and common debug issues are below:
This post applies to This post applies to ADS1191, ADS1192, ADS1291, ADS1292, ADS1292R, ADS1294, ADS1294R, ADS1296, ADS1296R, ADS1298, ADS1298R, ADS1299-4, ADS1299-6, and ADS1299.