Hello,
Now I met a stranger problem that the ADC result is randomly a larger number, while the corresponding input pin is empty.
My hardware connected 4 sensors, which is DC output, to TLA2024 4 inputs pins which are configured as single-end input mode, with 100ohm series resistor and 0.47uF parallel capacitor to GND as analog input filter, TLA2024 VCC=+5V, data rate = 1600 SPS, FSR set at ±6.144 V or ±4.096 V which depends on input level. Firmware control external sensors power on/off and TLA2024 to sample each channel one by one at single-shot mode.
When there is actual signal inputted, almost no problem, just start qualification now, but if there is no input, the actual case is the input port is empty by no connection for these corresponding ADC input ports, there is low chance that the ADC readout is a large number. Can somebody help to figure out what the problem of my design?
Thanks in advance!
Best Regards!
QM