Hi,
According to TI App Note SBAA161 (link at the bottom), for the RSC2007 it is required to have precise Ramp-on as well as ramp-off timing.
Three questions (can you please answer each of them separately):
1) to implement the first suggested solution in that application note with the switch switching between GND and VDD, what is the preferred/recomended switch to use? Can you please provide one or more part numbers.
2) The ramp-on and ramp-off timing would obviously be affected by the size of bypass capacitor on the VDD pin. How do we ensure that the ramp-on and ramp-off timing is achieved?
3) Because of point (2) above is the bypass capacitor better placed on the Vdd pin side of the switch or on the Rail side "before" the switch?
TI App. Note: http://www.ti.com/lit/an/sbaa161/sbaa161.pdf
Many thanks
Rick