Part Number: ADS8028EVM-PDK
Other Parts Discussed in Thread: ADS8028
Hi,
We have an ADS8028EVM-PDK board. And the SPI signals of the ADC EVM is connected to the external microcontroller. Whereas we want to use the power supply from the MMB0 board. As there are very few documentations about the MMB0, we don't know if we can do that. If we plug the EVM into the MMB0, the SPI signals are also routed to the pins of the controller on the MMB0. Is it possible to use the EVM with MMB0 and external microcontroller at the same time?
Thanks in advance!
Best regards,
Jianxiong