This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5401: ADC aperture delay?

Part Number: ADS5401

Hi,

What is the aperture delay - sampling clock rising (?) edge to the time when the actual sampling occurs, normalized to the input pins (actually balls)?  Can not find any related data in the datasheet besides 100fs rms aperture jitter. Is it reasonable to expect the delay stay more or less the same when sampling frequency changes and not subject to much variation between pin compatible parts (ADS540x) with different performance (500-800 Msps max)?

Regards,

Alexey