Part Number: ADS1247EVM
Other Parts Discussed in Thread: ADS1247, ADCPRO, MSP430F5529
Hi all,
I am setting up a temperature measurement with the ADS1247 EVM and PDK and a PT1000 in ratiometric setup (See TI document SLAU520A - 3-Wire RTD Measurement System Reference Design, -200°C to 850°C).
Visualising the data with ADCPro works properly, but I would like to make use of current chopping capability of this adc. Unfortunately the chopping functionality is not implemented in the GUI of ADCPro... So is there a way to implement the chopping with the EVM and PDK board? Or do I have to implement my own SPI communication?
Thanks for the help in advance
Kind regards, Dominik