Part Number: TSC2007
Hello TSC2007 Experts,
I found several units with an unresponsive touch screen.
When inspecting the units I noticed I can correctly access the TSC2007 via I2C but I got an almost stable value for X,Y and Z no matter where I touch the screen.
After some testing it has started working and it still does.
I was wondering if our setup is missing some initialization commands.
Is there any setting for the TSC2007 which might have an effect BETWEEN power cycles? Any register which is kept in a NVM?
The touch controller is connected to a I.MX cpu running Linux. During my test I did not use the touchscreen linux driver but I accessed the controller registers via i2c bus.