Part Number: ADS7949
According to the datasheet (with 10/12 bit info removed) "The ADS79479 is 8-bit 2MSPS analog-to-digital converters (ADC). Device operates at 2MSPS sample rate with a standard 16 clock data frame. In addition, it is possible to operate the the ADS7949 (8-bit) at 3MSPS with a short data frame optimized for the number of clocks sufficient for conversion with no drop in performance."
I am a bit confused how this 3MSPS operation works. Is there a way the ADC must be set up for 3MSPS operation? Can it continuously run at 3MSPS indefinitely? In short, what makes the product a 2MSPS ADC instead of a 3MSPS ADC if there is no drop in performance at 3MSPS?
I'm looking for an 8Bit (can't be higher) differential or Pseudo-Differential ADC with Serial SPI output and a high data rate (ideally >2MSPS) that is still low cost, hence this question.
Thanks!