Hello,
Could you provide an overview of TI's General Purpose ADC families?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Could you provide an overview of TI's General Purpose ADC families?
Hello,
You can access all of TI's <16-bit ADCs using the following search link:
http://www.ti.com/data-converters/adc-circuit/precision-adcs/products.html#p84=4.5;14
In addition to the full list, here is a high-level overview of several key families that focus on four important general purpose ADC features/vectors: Cost, Size, Ch Density, and integrated Diversified Features.
This slide provides an overview of two popular families and the combinations of channel, sample rate, and resolution offerings available in the families.
ADS7040, ADS7041, ADS7042, ADS7052, ADS7046, ADS7056, ADS7142, ADS7138, ADS7924, ADS8028, TLA2021, TLA2022, TLA2024, ADC128S102, ADS7958, ADS7954, ADS7950, ADS7959, ADS7955, ADS7951, ADS7960, ADS7956, ADS7952, ADS7961, ADS7957, ADS7953