This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J66: the question about SYSREF

Part Number: ADS54J66
Other Parts Discussed in Thread: LMK04828,

Hi,

I want to use gapped-period SYSREF.

so I configure the EVM board as follows:

step 1:

configure LMK04828. The config files are attached,whose name are' LMK_4421_mode8_pulser_LVDS_step1.cfg' and 'LMK_step2.cfg' seperately.

step2:

press the RESET button on the EVM

step3:

configure ADS54j66.The config file is attched,whose name is ADS54J66_bypass_4421_0_0p5fs.cfg.

step4:

configure RX EVM 

And the the link works OK. My question is :

The LMK04828 was configured before the reset of ADC, so the SYSREF pulses generated before the reset and configure of ADC.  And when ADC finished configuration, the SYSREF pulses has already disppeared. SO I think that once ADC has been powered up, even not be configured, ADS54j66 will be ready to receive SYSREF  pulses and will remerber it? Am I right?

Best Regards.LMK_4421_mode8_pulser_LVDS_step1.cfgLMK_step2.cfgADS54J66_bypass_4421_0_0p5fs.cfg