Part Number: DAC8831EVM
Other Parts Discussed in Thread: DAC8831, DAC8830,
When CS is low (so as to transfer new data with SPI), the DAC ouput falls down if the output was high and rises if the output was previously low.
All SPI timings are compliant with the datasheet.
SPI Clk is about 30MHz.