Part Number: ADS41B49
We are in the DVT process with a new board and are not able to get a high-speed differential clock output nor a SPI readback from the ADS41B49.
1. Output clock issue: We have a 192 MHz differential clock present at CLKP/M as driven by an FPGA, and verified on a scope. However the 192 MHz output differential clock isn’t being generated and output on CLKOUTP/N as verified on a scope.
2. SPI issue: SPI commands are coming from an ARM processor and verified on a scope to look correct. The ADC isn’t responding to SPI read-back commands, when theoretically it’s been put in READBACK mode.
To resolve both, we've tried initial HW reset on the RESET pin, as well as, a SW reset through the SPI interface. Neither makes a difference. All voltages and grounds to the chip appear correct. Please assist in resolving these issues.