I am using an ADC128S102QML-SP in an application where VA = 5Vdc and VD = 3.3 +/- 0.3Vdc. The datasheet only has two cases of VA=VD. What are the supply currents for my configuration?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using an ADC128S102QML-SP in an application where VA = 5Vdc and VD = 3.3 +/- 0.3Vdc. The datasheet only has two cases of VA=VD. What are the supply currents for my configuration?
Hello Thomas,
We do not have data for those exact conditions. Here are average data from one lot tested with a 16 MHz clock.
Clock = 16 MHz
Normal Mode +25C +125C
Vd @ 3.6V 1.1 mA 1.1 mA
Va @5.25V 0.06 mA 0.07 mA
Shutdown Mode
Vd @ 3.6V 88 nA 205 nA
Va @ 5.25V 0.003 uA 0.004 uA