Part Number: ADS131E08
Hi team,
Let me ask you basic question in terms of output code of ADS131E08 in case of Pseudo-Differential Input.
When AVDD=VREFP=2.5V/AVSS=VREFN=-2.5V and VINN=0V, full scale range should be ±2.5V because of Pseudo-Differential Input.
In this case, ADS131E08 can generate output code as 400000(-2.5V)~3FFFFF(2.5V).
Because when differential input, full scale output code should be 800000(-5V)~7FFFFF(5V).
So in case of Pseudo-Differential input, output code range is supposed to be half of differential input.
Is this understanding correct?
If so, in case of Pseudo-Differential input, 1LSB is NOT derived by (VREF / Gain) / 2^24 BUT (2 × VREF / Gain) / 2^24 even though full scale range of Pseudo-Differential is VREF.
Is this also correct?
I'm looking forward to hearing back from you.
Best regards,
Shota Mago