Hi Team,
I need to know how to activate the impedance in ADS1298 chip .
According to (9.3.1.7.4 Lead-Off Detection) in datasheet , I should be able to detect electrode connection ( on/off ) using LOFF_STATP and LOFF_STATN registers ,
I tried many values of registers 0x04,0x0f,0x10,0x11,0x12,0x13 and 0x17 and the result didn’t change .
Status word in return data is : 0xC0 0x0F 0xF0. Which mean the LOFF_STATP register not changes with value 1 for all channels .
The values of the registers which related to LEAD OFF are (what I think in order work ):
0x04 : 01111001
0x0F : 11111111
0x10 : 11111111
0x11 : 00000000
0x12 : default
0x13 : default
0x17 : 00000010
I would be thankful for any help .
Thanks,
Shlomi