Other Parts Discussed in Thread: SN74LVC244A
Tool/software: Code Composer Studio
Hi, I do plan to perform TC measurement using ADS1220. I have 8 ADS1220s that will communicate with the TIVA through SSI. I am looking for the best sequence without affecting the accuracy of my measurements. Initially, I was planning to start the ADC conversion on each ADS1220 and then for the next sweep I was planning to start the internal temp. conversion on each to perform CJC and get the final result. But, not sure this is best way because of the delay between ADC and int. temp sensor readings on each ADS1220. Would that delay effect the accuracy of my readings ? Thanks...