Part Number: TSW1400EVM
Other Parts Discussed in Thread: AFE5808, AFE5818EVM
Hello, I have the following problem I am trying to create an environment of study in the university to be able to acquire signals and later to be able to work with the obtained results. For this, I found it very interesting to use the AFE5808 and TSW400 cards from Texas, which as I can see, allow me to work easily with students through the use of LabVIEW. However, I found a problem that I did not have, the Trigger control. When I read the specifications of the TSW1400 card I noticed that I had an external Trigger, with which I thought I could launch the capture at the time I wanted, and I can effectively do it with the HSDC Pro program without any problem, but I just wanted to have the .dll libraries provided by Texas, without having to start the program every time. In this post I found the possibility of using the TSW1400Board_CLib.dll library that does not need to have previously released HSDC Pro, and I can create a simple LabVIEW program that acquires the signals, but nevertheless, I can not find the function that allows me to control the Trigger . I am only able to acquire signals continuously, but not at the time I request it. The only function that seems to allow controlling the Trigger is TSW1400BrdCtrl_Start_ADC_to_DDR, but I do not understand how it is used. My question is: Is it possible with this or another library to be able to control the trigger, without having to use HSDC Pro? I hope your answer. A greeting.