Other Parts Discussed in Thread: DAC38RF82, DAC38RF83
Looking over the documentation for the evaluation CCA for the DAC38RF82 we have come across discrepancies and wondering if you could clarify?
Figure 20 in SLAU671A (http://www.ti.com/lit/ug/slau671a/slau671a.pdfdoes not match the schematic provided for the DAC38RF8xEVM board. The resistor values for R211, R210, and R212 are not consistent between the two,. Looking at the BOM’s for the 6 different DAC options, they all agree with the Schematic and not Figure 20. We are wondering if the boards are built to the BOM’s or Figure 20? Additionally is the 16dBm input power based on the manual values for that input T attenuator. Our calculations show a difference of about 7dB between the different resistance values in those spots. I also notice the wording in 1.2.1.1 states that the default EVM is configured for single-ended clock but the schematic shows the single-ended path as DNI.
We are calculating that T1 should be driven between -1dBm and 7dBm based on the spec in the DAC38RF83 datasheet. Based on the values from the BOM what does TI recommend we drive the J1 clock EVM with?