Part Number: ADS1274
Other Parts Discussed in Thread: ADS1278
I would like to use ADS1274 with SPI interface. I would like to make sure to understand correctly table 7 of the datasheet.
Is it possible to use ADS1274 in high speed mode with a clock frequency (fclk) lower than 27MHz?
For example is it possible to operate in high speed mode with 10MHz fclk and therefore to consider the ratio (fclk/fdata) equal to 256? In this case fdata will be 39062 Samples Per Second and the signal passband will be 17.7kHz
Thanks in advance