Hi
When I went through the datasheet and application note, I found the bypass capacitors have been placed in the channel input lines.
If so is the case, then can ADS7953 read PWM signals (modulated at 200 Hz with variable duty cycle)?
Won't a pwm signal be filtered by low pass filtering due to the capacitors? If yes, can ADS7953 be used for reading PWM signals without the filters?