This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292R: Problem after calibration

Part Number: ADS1292R


Since I wanted to remove the DC offset, follow the calibration sequence.

***

Set the seventh bit of register 0Ah to 1 and send the command 'OFFSETCAL'.

Delay about 100 ms for the operating calibration (* Gain 6, SPS 500).

***

After that, I set up the registers to measure test signal that is AC 1 mV square wave with a gain of 6.

But the result is below ....

 I wanted a Square Wave with DC removed ... but it was not.

I do not think there is a problem with my code or register settings. This is because the test signal can be read before calibration.


(0x01, 0x82);
(0x02, 0xA3);

(0x04, 0x05);
(0x05, 0x05);
(0x06, 0x2F);
(0x0A, 0x82);

This register value was after calibration...
How can I solve this?



And one more,


I can read ECG signals with RLD. but the 60Hz power noise and significant DC components still annoy me....(I analyzed frequency of the signal in MATLAB)
How do I cancel these?