Part Number: ADS8664
Hi,
In ADS8664 datasheet chapter 7.1, there is an unclear description as below. please kindly explain what is this 30kΩ stand for? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yue Tang,
The condition 2) states the maximum input rating when AVDD(+5V) is available and the condition 3) states that the maximum input rating when AVDD is not present to the ADC.Since AVDD is applied to internal diodes for over-voltage protection(Figure 68), also the internal PGA provides a attenuation to input signal with RFB and 1Mohm input impedance. The absence of AVDD is similar as a high impedance status and an available AVDD shows a low impedance, the impedance on this node will have an influence on input attenuation. 30kohm is a simulation result as the conditions.
I hope this is helpful to you.
Thanks, Tom.
Best regards,
Dale