Part Number: DAC8771
Other Parts Discussed in Thread: LM25180
Hi,
This may be the cause of the failure.
At the same time, I will check again if the customer's DAC8771 is really broken.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC8771
Other Parts Discussed in Thread: LM25180
Hi,
Hello Hiroshi-san,
I received your PM and sent an email to the address you provided. We can continue to discuss on this E2E thread or over the email, whichever you prefer.
If PVDD/AVDD drops to this low below the recommended minimum operating voltage the device will likely reset, but this should not cause damage. I suspect this is what is happening and why you only see the issue when you 'hot' connect the DMM.
The power supply you are using can only support 33mA while the DAC8771 can consume an average DC current of ~100mA. You will need to use a different supply.
The peak inductor current of 500mA is supplied from the bypass capacitance so the supply does not have provide DC 500mA. I would target 150mA DC and add extra capacitance on AVDD/PVDD. I am not sure on specific power ICs so you can use the parametric search or post on the power management forum. In a reference design we recently did with DAC8771 we used LM25180 for an isolated supply. You can view the reference design at the link below.
http://www.ti.com/tool/TIDA-01535
Thanks,
Garrett
Hi Garrett-san,
Thanks a lot.