Part Number: ADS1220
-Sean
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1220
-Sean
Bob,
Below is the schematic for my setup. I will get some pictures of my setup as well and upload those. I understand what you are saying regarding the need to use both analog and digital power supplies and I am doing that now for all my testing.
I have tested with the analog and digital power supplies coming from the Raspberry Pi's 3.3V supply. I have also tested with the digital supply being sourced from the Raspberry Pi and the analog supply being generated by a separate bench top 3.3V supply. In all cases the ADS1220 will eventually reset during continuous data output mode and have all 4 of its registers reset to 0x00 values.
When I test with the Raspberry Pi driving the 3.3V digital supply and the analog supply being driven by an external bench top 3.3V supply I have discovered that if I disconnect the analog and digital grounds by removing R10 the sample rate drops to 5 SPS. If the analog and digital grounds are connected together (placing R10) the data rate returns to 20 SPS which is what I have set it to in the configuration registers. This behavior confuses me. But in either case the ADS1220 will eventually rest during continuous data output mode and the data ready line will stay high at 3.3V. When this occurs all 4 configuration registers will have been somehow been reset to 0x00.
I have managed to catch the SPI comms for the last valid query before the IC resets and the SPI comms look valid for clocking out the 24 bits of data. There is no reset command being sent by the Raspberry Pi at any time.
Thank you for your help and time.
-Sean
Hi Bob,
I may have figured out what the root cause is with my reset problem for the ADS1220 when communicating via the SPI bus using the Raspberry Pi. I think the issue has to do with the edge transitions on the MOSI pin while clocking out a sample during continuous sample mode. Currently the MOSI pin is transitioning low in between each of the 3 bytes read back from the ADS1220. This works for a while but eventually the ADS1220 resets. However if the MOSI line is tied high to 3.3V the part does not reset and I am able to clock out samples continuously without any issue. I ran a 24 hour test over the weekend and did not have any resets occur. Previously when the MOSI line was transitioning low in between each byte the system would reset after an hour or so of continuously reading data. I am currently testing to see if taking MOSI to GND while clocking out samples during continuous mode works without any reset events. I attached 2 images showing what I believe to be the problematic MOSI line transitions causing eventual resets of the part. On page 37 of the part's data sheet it shows the MOSI (DIN) pin being held at ground while continuously reading data. So I think the problem was that I was not properly implementing the SPI communications with the part with respects to the MOSI line while clocking out data in continuous mode.
thank you
-Sean
Hi Bob,
Sorry for the long delay in responding. I have done a lot of testing since my last post. You are correct that the issue was not what I thought it was with regards to the SPI comms protocol.
The issue was noise spikes on the +3.3V digital supply which occasionally were large enough to actually reset the ADS1220 part which of course cleared the 4 configuration registers. I was able to capture these events on an o-scope. The source of this noise is something I don't yet fully understand.
I did experiments where I used 3 separate isolated lab grade power supplies. One powered the Raspberry Pi, the other powered the digital side of the ADS1220 and the 3rd supply powered the analog side of the ADS1220. I tied all three grounds together at the supplies. My O-scope was running of a 1:1 isolation transformed and I removed the Raspberry Pi's HDMI connection to a monitor so as to prevent any ground loops. Even in this configuration there were still noise spikes on the ADS1220 digital side which would occasionally reset the part.
So I added 100uF tantalum caps on both the digital and analog power supply inputs to the ASD1220 part. This has resolved the issue but not completely as I would like. There does seem to be a noise component from the SPI clock that correlates closely with the other SPI lines as well as the digital power supply to the ADS1220. But these noise spikes occur when the SPI clock switches states and are small in amplitude. The spikes that occur on the digital supply to the ADS1220 which can rest the part don't seem to be directly correlated with the SPI comms and are much larger then the ones that correlate with the SPI clock switching rates.
I have also experimented with disabling the wifi and bluetooth module on the Raspberry Pi to see if that made a difference in the spike events... but it did not make any difference unfortunately. So I don't totally understand the source of these spikes on the +3.3V digital side of the ADS1220... but adding 100uF caps has resolved the issue. I am now powering the Raspberry Pi with a single supply and using its 3.3V output to drive both the digital and analog sides of the ADS1220 part. With the addition of the 100uF caps this is working and no reset events have occurred over several days of continuous operation.
I included an updated and corrected schematic. This new schematic has the following changes...
1. includes the 100uF tantalum caps on the digital and analog power supplies to the ADS1220 part
2. corrects a mistake in my earlier posted schematic regarding the smaller C1 and C2 caps
3. The chip select pin is now taken to the Raspberry Pi's SPI bus 0 dedicated CS0 pin 24. Previously I was using a digital I/O for CS and not taking advantage of the dedicated CS pin built into the SPI bus 0 hardware
For my setup I am using a small proto-board I purchased from ProtoCentral which has the ADS1220 part. I mounted this module to some strip board and have a very short cable (~3") for the SPI bus and power from the Raspberry Pi. I will post a picture. My SPI clock rate is set to 7629 Hz.So at this point the 100uF capacitors appear to be working and preventing resets of the part... but I will continue to try and track down the ultimate cause of the random noise events on the digital supply to the ADS1220.
thank you
-Sean