Part Number: TSC2004
Dear all,
Would you mind if you ask for Stabilization time(tpvs) and Internal Clock?
Our customer would like to know about deviation of Stabilization time tpvs and Internal Clock.
Could you answer the following questions?
1. Is Stabilization time (tpvs) affected by the internal clock in TSC2004?
2. Could you tell me the deviation of Stabilization time tpvs=10ms and Internal Clock under the following situations?
- tpvs=10ms (PV2=1,PV1=0,PV0=1)
- Supply Votage (SNSVDD):3.3V±7%
- Ambient Temperature:-20℃~60℃
it would be great if you could let me know your thoughts on the following the questions.
Best regards,
Y.Ottey