Hi all,
We have developed a ECG monitoring device in which ADS1292 is used as an AFE,but the device failed the IEC 60601-2-47 (ambulatory ECG device) test but we passed all other tests I have some questions related to this test
1. why it is called input impedance test ?
2. while selecting this test the test device (SECG 4.0) will add a 620K in series and 4.7nf parallel to the circuit(LOW pass filter) what is the purpose of this?
can anybody tell what is the basic idea of this test?