Part Number: ADS130E08
Other Parts Discussed in Thread: ADS124S08
Hello,
Please tell me about ADS130E08.
This device can be used as fully differential or pseudo differential,
Customers use it as pseudo differential.
INxN inputs 1.65V. And INxP is input from 0V to 3.3V.
AVDD = 3.3V, AVSS = 0V, VREF = 3.3V (Vrefp-Vrefn = 3.3V-0V)
I confirmed the data sheet. The datasheet shows the analog input as ± VREF / gain. And its VREF is AVSS-0.3V to AVDD + 0.3V.
In this context, the analog input is in the 0V to 3.3V range.
It looks like you can enter it.
on the other hand
I confirmed the contents of the Input Common-Mode Range in the data sheet.
When AVDD = 3.3 V, AVSS = 0 V, and Vmmax_diff is 3.3 V
Inequality does not hold.
AVDD-0.2-(GainVmax_diff / 2)> CM> AVSS + 0.2 + (GainVmax_diff)
Both full differential and pseudo differential
Is the valid analog input range from 0.2V to 3.1V?
Best regards,
DDdoor