I have an existing DAC/ADC solution with an external +/- 15V buck-boost providing the positive and negative analog supplies for both.
I'm hoping to switch to the DAC8775 for the additional channels. With the integrated buck-boost, it would be very nice if I could get rid of the external buck-boost as well. The one issue is the ADC.
I've combed through the manual and couldn't find any mention of using one of the channel's buck-boost to power external circuitry. Assuming issues such as power supply sequencing, noise, etc. for the ADC are not an issue, is there any problem using one of the channel's buck-boost to supply the ADC?