Other Parts Discussed in Thread: ADS1261, ADS1282, ADS1248
Hi team,
For ADS1256, from datasheet, we can see it has internal full scale calibration function, which can connect internal voltage to input, and improve PGA gain error greatly after calibration. For G=1, I can understand how it works(apply reference voltage to input, then measure output), but for G>1, I don`t know how ADS1256 realize the calibration, because we need to set lots of accuracy voltage source in the device, like Vref/2, Vref/4,…Vref/128, and you know it`s quite difficult to create accuracy divider circuit in device. So could you have comments on how ADS1256 complete gain error calibration(internal full scale calibration) at all different gain?
And another question is: I found lots of other SD ADC, like ADS1248/ADS1261/ADS1282, it doesn`t has internal full scale calibration, if you need to calibrate the gain error, you must use system full scale calibration, that means you need to add external accuracy input by yourself. Do you know why these devices doesn`t has internal full scale calibration while only ADS1256 support that?
thanks very much.
Regards, Sunny