Part Number: ADS1248
Other Parts Discussed in Thread: ADS1220,
Hi all,
the output voltage of the internal temperature sensor is typical 118mV @ 25°C. What is the min. and max. output voltage at 25°C?
Thanks a lot!
Best regards, Xaver
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Xaver,
It is possible to calibrate but this would have to be done for each device as there will be device to device variation as well as lot to lot variation. This variation could be in the range of 3 to 6 deg C. Also, the temperature is the die temperature. There could be some variation relative to ambient or board temperature with respect to die temperature.
You would need at least 2 known points for calibration to determine the coefficient. So a single measurement at 25 deg C will only give you a voltage at 25 deg C. The second point measurement would give you the value for the slope of the difference between the two temperatures.
Coefficient = (Vtemp2 - Vtemp1)/(Temp2 - Temp1)
Best regards,
Bob B