A working design we have had since 2015 which has the ADC12D500RF and recording the I and Q channels are showing an odd behavior we have never seen. The output of the ADC is identical of each channel, even though the inputs have been verified to be different. Is there some mode that the ADC is in that is causing this, possibly a voltage on one of the pins? I have the serial clock select held high since we are not using the serial communications. The ADC is to had DDRPH to logic 1, both I/Q channels enabled (logic 0), non-demux mode enabled, and DES mode disabled.
Any ideas?