Other Parts Discussed in Thread: ADS1299, , ADS1294R, ADS1296R, ADS1296, ADS1298
The ADS1299 seems to be lower noise than the ADS1298R and seems to be well suited for EEG but could also be used for EMG/ ECG.
The ADS1298R seems to be well suited for ECG.
When I skim through the datasheet of the ADS1298R I find quite a bit of ECG features built into the device like WCT, Pace detection, Respiration, Augmented leads acquisition in hardware.
I don't see these in the ADS1299.
We would have liked to have a common piece of hardware and develop around the ADS1299 to build a EEG/ECG/EMG.
I guess to get these same features as the ADS1298R in the ADS1299 would required extra hardware, correct?
Is the ADS1298R better suited for building a ECG vs the ADS1299? If so, we may have to develop 2 sets of hardware one around the ADS1298R for the ECG and one around the ADS1299 for EEG / EMG.