Part Number: ADS124S06
Other Parts Discussed in Thread: ADS124S08
For the ADC ADS124S06, the GPIO pins (GPIO0-GPIO3) are connected to the Input multiplexer block.
The specification states the leakage current for the analog pins AIN0-AIN5 at <2nA (Temp Ambient = –50°C to +125°C)
I am looking to connect the GPIOX pins to the AINX for connected input sensor health checks.
What is the off state leakage current for the GPIOX pins, is it a similar level to the AINX on state leakage pin at <2nA as it is connected to the input multiplexer and the device is a reduced feature variant of the ADS124S08 ?
Are there any figures for the "off" state leakage current of the AINX and GPIOX the data sheet only lists the "on" state leakage currents ?