Part Number: ADS1262
Other Parts Discussed in Thread: OPA388
Hello
I´m using the ADS1262 and I have a doubt about its resolution and dynamic range.
With a PGA set on Gain 32 and a reference voltage of 5V, the full scale range is 156mV. I ´m connecting to the ADS1262 a load cell of 100kg with 2 mV / V and it is excited with 5V. So the max. output of the load cell is 10mV.
The ADC and the load cell are connecting in ratiometric connection.
With this configuration does not take advantage of the capabilities of the ADC, due to the most part of the dynamic range does not be used.
I have some questions with respect to this:
- I would like to know how can I calculated the value of a 1 LSB and the quantification error for this configuration? 1LSB=FSR/2^n, but with this configuration, FSR is 156mV or it is continuing being 5V.
- With this configuration is only used 6.4% of the dynamic range (156mV=100%; 10mV=6.4%), is this mean that if for 156mV it is had 32 bits, for 10mV it is had only 2 bits (the 6.4% of 32bits)?
Apart of this questions...
Normally in this type of systems the correct way of increase the resolution is to adapt the range of the input signal to the range of the input ADC. To reach this it is neccesary for example use an instrumentation amplificator. I did this experimentally, but the read values were worse that without amplifier. Why the ADS1262 works better without a previous amplifier stage?
I read this post but I don't understand it good. http://e2e-ti-com.telligentsaas.net/support/data-converters/f/73/t/769753
Thanks in advance,
Best regards.