This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292R: ADS1292r

Part Number: ADS1292R

Dear sir:  we use adruino open source code and circuit for ads1292r ECG solution

              i ca'nt find ecg wave for ads1292r pin 7,8

             i think it is possible we can'nt read/write ads1292r reg.correctly

            so, i need to write value to ads1292r and the read it back to approve hardware ok

                       but, arduino code have no read reg function , only read data function

        could you help us to support how to  build read/write reg function  to approve our hardware and get ECG signal from pin7,8

      you can get source code for ads1292r easily i thank

     my e_mail:mingjerlin2010@gmail.com