This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1015-Q1: Operation Verification

Part Number: ADS1015-Q1


Hi,

I received the following question from my customer.

Has the ADS1015-Q1 been verified working on the all operate junction temperature and all Supply voltage?

They don't require guarantee, however they would like to confirm if it has been verified.

Best Regards,

Kuramochi

  • Kuramochi

    If you look through the characteristic curves you can see many curves were measured from -40C to 140C at 2V and 5V. Below is a typical example. So, yes, key parameters and functionality were tested and high and low supply across the temperature range.

     

    Best regards,

    Art Kay