Hi There,
While checking the datasheet some details are not available like VOH ,Acquisition time. Can anybody share the details. Want to have it for dc analysis.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi There,
While checking the datasheet some details are not available like VOH ,Acquisition time. Can anybody share the details. Want to have it for dc analysis.
Hello.
The VOH is your VDD power supply .
The acquisition depends on what communications mode you will be using. The below figure shows the beginning of the acquisition time at the 4bit of the command byte until you begin reading.
Note, in High speed mode, the clock is pulled low by the device until you are able to read out the results.
Regards,
Cynthia
Hi Cynthia,
Im planning to use this IC for thermistor based temperature sensor. So for this ADC IC we may use Fast Mode and High speed mode for this but not sure. If there source resistor and by pass cap is fixed then the acquisition time may get vary depends on mode we choose. Also do we need to have any special filter for this analog input. We thought of using RC filter but it will indirectly affect the acquisition time. Can you provide some suggestion here.
Hi Cynthiya,
We are planning to use either standard or fast mode for our application. Is there any possibilities to change the sampling rate? since datasheet not having much details compare to other datasheet.
For now considering 50KHz Sampling rate and through put @400KHz.
Attaching circuit for reference purpose.